DigiKey-eMag-Tools, Test and Measurement-Vol 20

Spectrum analyzers

Benchtop models typically outperform their handheld counterparts but can carry a higher price tag.

analyzer allows users to “analyze a spectrum,” where a spectrum is defined as a collection of sine waves combined to produce a time- domain signal. As an example, let’s observe a signal on an oscilloscope (Figure 2). While this signal is obviously not a pure sinusoidal waveform, a spectrum analyzer determines each of the individual sinusoidal waveforms that make up this signal. And after the spectrum analyzer has identified these waveforms, it plots the amplitude versus frequency of each individual waveform. As you can see in Figure 3, the signal from Figure 2 is made up of only two sinusoidal waveforms. Types of spectrum analyzers: technology types and form factors There are two main categories of spectrum analyzers: swept-tuned

analyzers are simply those (including some benchtop versions) that can be taken into the field thanks to their battery packs.

Unlike swept-tuned spectrum analyzers, real-time spectrum analyzers can evaluate all frequencies simultaneously. A real-time spectrum analyzer works by first acquiring data in the time domain and then converting that data into the frequency domain by use of the fast Fourier transform (FFT). Spectrum analyzers come in a variety of form factors, including benchtop (Figure 4), handheld (Figure 5), and portable. Benchtop models typically outperform their handheld counterparts but can carry a higher price tag. Handheld spectrum analyzers are both less expensive and smaller, but they offer only a subset capability relative to benchtop analyzers. Portable

Conclusion

While all (we hope!) electrical engineers know what an

Figure 5: Seeed Technology’s RF Explorer Model 2.4G is a 2.35 to 2.55GHz Handheld Spectrum Analyzer. Image source: Seeed Technology However, just like oscilloscopes, various spectrum analyzer types are available depending on one’s needs and budget.

oscilloscope is and how to use one, it can be surmised that only some electrical engineers have ever used a spectrum analyzer. Although oscilloscopes and some spectrum analyzers (the benchtop versions) may look similar in both form factor and display, they are quite different; a spectrum analyzer presents its acquired data in an amplitude-versus-frequency fashion, whereas an oscilloscope displays its information in an amplitude-versus-time method.

Figure 2: A signal displayed on an oscilloscope Image source: Agilent Technologies [3]

analyzers and real-time analyzers, also referred to as real-time spectrum analyzers, or RTSA. Both types, which have been used for many years, display amplitude on the vertical axis and frequency on the horizontal axis, but how they

go about “analyzing a spectrum” is what distinguishes them. Given that a swept-tuned spectrum analyzer is “nothing more than a frequency-selective voltmeter with a frequency range that’s tuned (swept) automatically,”[4] it’s not at all surprising to realize that these traditional types of analyzers “descended from radio receivers.”[4] And because swept- tuned spectrum analyzers “cannot evaluate all frequencies in a given span simultaneously,”[4] they are primarily used for measuring steady-state or repetitive signals. These analyzers have successfully served the compliance engineering community (think pre-compliance testing and EMC/EMI testing) for several decades.

References

1. Rigol Technologies, “ DSA800 Spectrum Analyzer Datasheet” (page 3) 2. Keysight Technologies, “What is a Spectrum Analyzer?” 3. Agilent Technologies, “Agilent Spectrum Analysis Basics” (pages 4-5)

4. Keysight Technologies,

“Different Types of Analyzers”

5. Teledyne LeCroy, “T3SA3100/ T3SA3200 Data Sheet” (page 2)

Figure 3: Relationship between a time domain signal (of which is displayed on an oscilloscope) and frequency domain signals (of which are displayed on spectrum analyzers) Image source: Agilent Technologies [3]

Figure 4: Teledyne LeCroy’s T3SA3200 Benchtop Spectrum Analyzer offers a frequency range from 9kHz to 3.2GHz. Image source: Teledyne LeCroy [5]

we get technical

14

15

Powered by