DigiKey-eMag-Exploring the Control Cabinet-Vol 21

In industrial environments, electrical cabinets remain one of the most dangerous points of contact for workers. Even when the power is shut off, residual voltage or partial disconnect switch failures can leave components energized. Each year, hundreds of arc flash events and electrical injuries occur because someone assumed the cabinet was safe to open. Workers must verify the absence of voltage before accessing electrical enclosures. However, traditional methods using handheld test instruments are complex and time-consuming. Even permanent tools like voltage indicators and test portals can fall short when it comes to confirming true de-energization. That’s where absence of voltage testers (AVTs) come in. These systems automate the verification process, giving workers a clear indication—without opening the enclosure—whether it is truly de-energized. This article explores the risks associated with conventional verification methods, and how Panduit’s VeriSafe AVT addresses their shortcomings. The problem with traditional methods Industrial workers rely on a variety of tools to assess electrical safety, but not all are designed— or approved—for verifying the

absence of voltage. Among the most commonly used are voltage indicators and test portals. While both offer some insight into the electrical status of equipment, they each carry limitations that can compromise safety when used for absence of voltage verification. Voltage indicators are simple, permanently mounted devices that illuminate when voltage is present, typically between 40V and 1000V. While they offer a quick visual warning, they are fundamentally limited when it comes to confirming de-energization. A non-illuminated indicator doesn’t necessarily mean the system is safe; LED or fuse failures, poor installation, or open circuits can all produce a false negative. Additionally, since these devices route line voltage directly to the enclosure door, they introduce a potential shock hazard when a worker is troubleshooting with the door open. OSHA has stated that voltage indicators should not be used to verify de-energization. Test portals offer another option. These devices allow technicians to connect a handheld tester to measure voltage without opening the cabinet. While helpful for troubleshooting, test portals are not well-suited to confirming a safe- to-open condition. They cannot verify that the internal leads are properly connected at the time of testing and are vulnerable to fusing issues. Either condition could show a zero-voltage reading when

voltage is actually present. Like indicators, test portals can also route hazardous voltage to the door, exposing workers to additional risk. Neither voltage indicators, nor test portals satisfy NFPA 70E’s requirements for absence of voltage verification. According to Article 120.5(7), proper verification must include testing each phase both phase-to-phase and phase-to- ground, using an adequately rated instrument. Exception 1 allows for permanently mounted test devices, but only if they meet strict criteria. Devices must be UL 1436 listed, test all phases, and perform self- verification using a known voltage source before and after testing. Both voltage indicators and test portals do not fulfil these conditions. While OSHA does not define detailed performance requirements

for voltage testing tools, it recognizes NFPA 70E as the

benchmark for electrical safety. By that standard, absence of voltage testers are the only permanently mounted device currently aligned with both best practices and regulatory expectations.

Introducing absence of voltage testers

Absence of Voltage Testers offer a streamlined, automated approach to verifying that electrical equipment is de-energized before access. Unlike voltage indicators

we get technical

5

Powered by