DigiKey-eMag-Exploring the Control Cabinet-Vol 21

Cabinet safety – A paramount consideration in any industrial application

or test portals, which either show the presence of voltage or allow indirect measurement, AVTs are dedicated safety devices built to verify that no voltage is present inside an enclosure. The core advantage of AVTs is that they automate a process that would otherwise require multiple steps and tools. At the push of a button, the system initiates an internal sequence: it checks that the tester itself is functioning, verifies that sensor leads are properly connected, tests each phase both phase-to-phase and

phase-to-ground, and uses a known voltage source before and after each test to verify the tester is functioning correctly. If all criteria are satisfied, a visual indication is provided to confirm that the absence of voltage has been verified. This automation reduces the chance of human error and eliminates the need to open the cabinet for initial testing. Industrial electrical manufacturer Panduit offers their VeriSafe Absence of Voltage Tester as one such solution. Once installed, it allows a qualified worker to initiate

the test sequence from outside the enclosure. By automating each verification step and providing a clear green-light indication when the system is de-energized, VeriSafe helps support safety without requiring handheld testers or direct exposure to conductors. The hardware behind Panduit’s VeriSafe AVT The VeriSafe AVT is designed around a modular architecture that separates operator interaction from high-voltage components,

Comparison of testing methods. (Image source: Panduit.)

6

Powered by