DigiKey-emag-IoT-Vol-2

How to quickly connect IoT nodes to Amazon AWS and Microsoft Azure Clouds

edited and debugged. The included application notes provide details of the operation of the applications. The sample programs are ported based on Amazon FreeRTOS and can be freely expanded, changed, and deleted using available source code libraries. The kit has AWS qualification, so it can communicate with AWS safely and securely and includes (Figure 5): ■ Cloud option board with temperature/humidity sensor, light sensor, and 3-axis accelerometer, plus a USB port for serial communication and a second USB port for debugging ■ Wi-Fi communication module based on the Silex SX-ULPGN Pmod module ■ All necessary power management ■ RX65N target board that Figure 4: Developers can use the eval boards in the RX65N Cloud kit to quickly implement IoT devices with connectivity to the Amazon AWS and Microsoft Azure Clouds. Image source: Renesas

IoT Node

Cloud Server

User Apps

Evaluation Board

Web Dashboard

of the world. Both provide quick connectivity to the Amazon AWS and Microsoft Azure Clouds (Figure 4). Using these kits, designers who do not have previous experience with developing IoT devices can quickly start using a solution in a Cloud connection environment. The RX65N Cloud kit supports flexible development with several sensors, user interfaces, and communication functions. It also provides sample programs to speed application development. The sample programs can be

customer audits of data hosted in a multiparty, Cloud environment using virtualised servers can be technically challenging and increase risks to existing physical and logical network security controls. The standard has several advantages, including: ■ Increased security for customer PPI data and information ■ Increased platform reliability for Cloud users and customers ■ Helps speed deployment of global operations ■ It defines legal obligations and protections for Cloud providers and users ■ MCU-based Cloud connection dev platform The RX65N Cloud kit from Renesas provides a platform for designers of industrial and building automation, smart home, smart meters, office automation, and general IoT applications to prototype and evaluate IoT equipment. Two variations are available: the RTK5RX65N0S01000BE, which supports development of systems for use in the US, and the RTK5RX65N0S00000BE for the rest

Digital 3.3V

5V

Cloud

ISL80019 Buck Regulator

USB

Wi-Fi

UART

Wi-Fi Module Silex

RX65N MCU

ISL9021A LDO

I2C

Analog 3.3V for Sensor

Humidity & Temperature Sensor

ISL29035 Light Sensor

ZM0D4410 Gas Sensor

HS3002

Figure 5: The RX65N Cloud kit is AWS-qualified and includes everything needed to connect IoT devices securely. Image source: Renesas

48

Powered by