DigiKey-emag- Edge AI&ML-Vol-10

Why and how to use Efinix FPGAs for AI/ML imaging – Part 2: Image capture and processing

The use of the DMA also enables the Sapphire SoC RISC-V to access the images stored within the frame buffer, and the abstract statistics and image information. The Sapphire SoC is also able to write overlays into the LPDDR4x so that they can be merged with the output video stream. Modern CMOS image sensors (CISs) have several modes of operation and can be configured to provide on-chip processing, and several different output formats and clocking schemes. This configuration is normally provided over an I²C interface. In the Efinix reference design, this I²C communication to the MIPI cameras is provided by the Sapphire SoC RISC-V processor. Integration of the RISC-V processor within the Titanium FPGA reduces the overall size of the final solution as it removes the need to implement both complex FPGA state machines that increase design risk, as well as external processors that add to the BOM. Inclusion of the processor also enables support with additional IP to communicate with the MicroSD card. This enables real-world applications where images may be required to be stored for later analysis. Overall, the architecture of the Ti180 reference design is optimized to enable a compact, low-cost, yet high-performance solution that allows developers to reduce BOM

to the sensor’s output. These functions can include Bayer

The Ti180 M484 reference design clearly showcases the capabilities of Efinix FPGAs and the Ti180 in particular. The design leverages several of the unique I/O structures to implement a complex image processing path that supports several incoming MIPI streams.

conversion, auto white balance, and other enhancements. In the output stream, the image is prepared for display. This includes changing color spaces (e.g., RGB to YUV) and post-processing for the desired output format, such as HDMI. Often the input image processing chain operates at the sensor pixel clock rate. This has different timing to the output chain, which is processed at the output display frequency. A frame buffer is used to connect the input to the output processing pipeline, which is often stored in external high-performance memory, such as LPDDR4x. This frame buffer decouples between the input and output pipelines, allowing access to the frame buffer via direct memory access at the appropriate clock frequency. The Ti180 reference design uses a similar approach to the concepts outlined above. The input image processing pipeline implements a MIPI Camera Serial Interface 2 (CSI-2) receiver intellectual property (IP) core, which is built upon the MIPI physical layer (MIPI D-PHY)-capable input/ output (I/O) of the Titanium FPGA. MIPI is a challenging interface because it uses both single-ended and differential signaling on the same differential pair, in addition to low-speed and high-speed communications. Integrating the

MIPI D-PHY within the FPGA I/O reduces the complexity of the circuit card design while also reducing the bill of materials (BOM). With the image stream from the camera received, the reference design then converts the output of the MIPI CSI-2 RX into an Advanced eXtensible Interface (AXI) Stream. An AXI Stream is a unidirectional high-speed interface that provides a stream of data from a master to a slave. Handshaking signals to transfer between a master and slave are provided (tvalid and tready) along with sideband signals. These sideband signals can be used to convey image timing information such as start of frame and end of line.

converted into an AXI Stream and input into a direct memory access (DMA) module, which writes the image frame to the LPDDR4x and acts as the frame buffer. This DMA module is operating under the control of the RISC-V core in the FPGA within a Sapphire system on chip (SoC). This SoC provides control, such as stopping and starting DMA writes, in addition to providing the DMA write channel with the necessary information to correctly write the image data to the LPDDR4x. This includes information on the memory location and the width and height of the image defined in bytes. The output channel in the reference design reads the image information from the LPDDR4x frame buffer under the control of the RISC-V SoC. The data is output from the DMA IP as an AXI Stream, which is then converted from RAW format provided by the sensor to RGB format (Figure 2), and prepared for output over the on-board Analog Devices’ ADV7511 HDMI transmitter.

Figure 2. Sample images output from the reference design. Image source: Adam Taylor

At a high level, this application may appear to be straightforward. However, receiving multiple high- definition (HD) MIPI streams at a high frame rate is challenging. This is where FPGA technology is beneficial because it allows designers to utilize multiple MIPI streams in parallel. The architecture of the reference design leverages both parallel and sequential processing structures with the FPGA. The parallel structures are used to implement the image processing pipeline, while a RISC-V processor provides the sequential processing used for the FPGA look-up tables (LUTs). The image processing pipeline can be split into two elements within many FPGA-based image processing systems, namely the input and output streams. The input stream is connected to the camera/sensor interface, and processing functions are applied

The Ti180 M484-based reference design

Conceptually, the reference design (Figure 1) receives images from several Mobile Industry Processor Interface (MIPI) cameras, performs frame buffering in the LPDDR4x, and then outputs the images to a High Definition Multimedia Interface (HDMI) display. An FPGA Mezzanine Card (FMC) and four Samtec QSE interfaces on the board are used to provide the camera inputs and HDMI output. The FMC to QSE expansion card is used in conjunction with the HDMI daughter card to provide the output video path, while three QSE connectors are used to interface with the DFRobot SEN0494 MIPI cameras. If multiple MIPI cameras are not available, a single camera can be used by looping back the single camera channel to simulate additional cameras.

AXI Stream is ideal for image processing applications and

enables Efinix to provide a range of image processing IP which can then be easily integrated into the processing chain as required by the application. After being received, the MIPI CSI-2 image data and timing signals are

we get technical

52

53

Powered by