DigiKey-emag- Edge AI&ML-Vol-10

How to run a ‘Hello World’ machine learning model on STM32 microcontrollers

Machine learning (ML) has been all the rage in server and mobile applications for years, but it has now migrated and become critical on Edge devices. Given that Edge devices need to be energy efficient, developers need to learn and understand how to deploy ML models to microcontroller-based systems. ML models running on a microcontroller are often referred to as tinyML. Unfortunately, deploying a model to a microcontroller is not a trivial endeavor. Still, it is getting easier, and developers without any specialized training will find that they can do so in a timely manner.

The next use case for tinyML that many embedded developers are interested in is image recognition. The microcontroller captures images from a camera, which are then fed into a pre-trained model. The model can discern what is in the image. For example, one might be able to determine if there is a cat, a dog, a fish, and so forth. A great example of how image recognition is used at the edge is in video doorbells. The video doorbell can often detect if a human is present at the door or whether a package has been left. One last use case with high popularity is using tinyML for predictive maintenance. Predictive maintenance uses ML to predict equipment states based on abnormality detection, classification algorithms, and predictive models. Again, plenty of applications are available, ranging from HVAC systems to factory floor equipment. While the above three use cases are currently popular for tinyML, there are undoubtedly many potential use cases that developers can find.

Introduction to tinyML use cases TinyML is a growing field that brings the power of ML to resource and power-constrained devices like microcontrollers, usually using deep neural networks. These microcontroller devices can then run the ML model and perform valuable work at the edge. There are several use cases where tinyML is now quite interesting. The first use case, which is seen in many mobile devices and home automation equipment, is keyword spotting. Keyword spotting allows the embedded device to use a microphone to capture speech and detect pretrained keywords. The tinyML model uses a time- series input that represents the speech and converts it to speech features, usually a spectrogram. The spectrogram contains frequency information over time. The spectrogram is then fed into a neural network trained to detect specific words, and the result is a probability that a particular word is detected. Figure 1 shows an example of what this process looks like.

Written by: Jacob Beningo

This article explores how

embedded developers can get started with ML using STMicroelectronics’ STM32 microcontrollers. To do so, it shows how to create a ‘Hello World’ application by converting a TensorFlow Lite for Microcontrollers model for use in STM32CubeIDE using X-CUBE-AI.

Figure 1. Keyword spotting is an interesting use case for tinyML. The input speech is converted to a spectrogram and then fed into a trained neural network to determine if a pretrained word is present. Image source: Arm

we get technical

8

9

Powered by