DigiKey-eMag-Sustainability and Energy Harvesting-Vol 15

Resources i. https://nam.org/sustainability-is- a-top-manufacturer-priority-survey- shows-19992/?stream=business- operations ii. https://unfccc.int/process-and- meetings/the-paris-agreement iii. https://zerotracker.net/analysis/ new-analysis-half-of-worlds-largest- companies-are-committed-to-net-zero iv. https://nam.org/sustainability-is- a-top-manufacturer-priority-survey- shows-19992/?stream=business- operations v. https://gaoinnovations.gov/ Federal_Government_Contracting/ vi. https://ec.europa.eu/ commission/presscorner/detail/ en/IP_23_1665 vii. https://iea.blob.core.windows.net/ assets/98909c1b-aabc-4797-9926- 35307b418cdb/WEO2019-free.pdf viii. https://new.abb.com/news/ detail/75020/abb-urges-greater- adoption-of-high-efficiency- motors-and-drives-to-combat- climate-change-global-electricity- consumption-to-be-reduced-by-10 ix. https://www.analog.com/media/ en/technical-documentation/data- sheets/max17692a-max17692b.pdf

Figure 2: ADI's EVAL- ADM3066EEBZ evaluation board has a footprint for the ADM3066EBRMZ half-duplex RS- 485 transceiver in a 10-lead MSOP package. (Image source: Analog Devices, Inc.)

Building automation systems typically incorporate multiple

Conclusion The growing demand for net- zero sustainability by 2050 represents an enormous opportunity for products that support manufacturing innovation, retooling, and advancing new technologies. While 2050 may seem far in the distance, data cited in this article underscores that governmental, business, and societal pressures are already causing many companies to build 2050 net-zero and 2030 carbon-neutral goals into their current strategies. Every supplier ultimately will likely need to show progress toward those goals. Product designers who proactively incorporate those goals into their planning, processes, and component supplies stand to benefit from one of the largest industrial transformations ever.

controllers and disparate nodes, each requiring reliable connectivity. The ADIN1110 is a low-power single-port transceiver with an integrated media access control (MAC) interface that requires lower overall system-level power consumption, and has integrated voltage supply monitoring and power-on reset circuitry to improve system-level robustness. Intelligent buildings need efficient management of power at the edge. ADI's LTC4296-1 enables Single-pair Power over Ethernet (SPoE) power sourcing for 10Base-T1L controllers and switches, with transmission of up to 52 W of power plus data over a single twisted-pair Ethernet cable. The LTC9111 is an IEEE 802.3cg-compliant SPoE power device controller particularly suited for classification-based systems in building and factory automation.

we get technical

67

Powered by