DigiKey-emag-Adv-Future-Automation-Vol-3

How Delta Robotics Optimize and Streamline Electronics Manufacturing Processes

industrial robot manufacturers that primarily produce articulated- arm robots. The supplier’s delta robots offer payloads of 1.5 to 125 kg to execute the assembly of tiny electronic parts to many designs far larger. A Mitsubishi Electric partnership pairs Codian delta robots with Mitsubishi controllers. ABB’s delta robots are produced under the FlexPicker brand. The current model is the IRB 360, a delta robot with two auxiliary rotary axes in series at the end effector for five-axis motion. These robots are optimized for pick and place operations. Fanuc produces delta robots in two ranges. The M-series includes small robots used for assembly of small parts (most commonly electronics) as well as larger robots. M-series robots are available in three, four, and five-axis configurations. The DR-3iB series robots are larger four- axis robots designed for picking and packing operations, with motion speeds of up to 5.5 m/sec and payloads up to 8 kg. Conclusion Delta robots provide affordable and flexible automation for electronics manufacturing. They often provide higher speed and more flexibility than other robotics and automated pick-and-place machines.

Figure 6: Some delta robots maneuver through five axes to orient objects of all types. The IRB 365 shown here can sort, feed, pick, reorient, and place 1-kg products at 120 picks per minute — satisfying the requirements of production facilities needing high throughput and efficiency. Commanded by a compact delta- robot controller called the OmniCore, the system offers performance motion control, digital connectivity, and more than a thousand programmed functions. (Image source: ABB)

dominate for smaller components; they’re much better suited to highly automated volume manufacturing. That said, some through-hole mounting is often still required for larger components such as capacitors, transformers, and connectors. For both kinds of PCB component attachment, machine vision complementing a delta robot can check the component variation and orientation before installation on the board. For high throughput, the robotic pick-and-place head may be designed to process several components at a time. A robotic end effector may also apply solder paste, and yet another may apply

heat to electrically connect the installed components. Otherwise, components may be attached by a wave-soldering technique … though machines for this are expensive and best suited to very high-volume manufacturing. Even costlier is how components too large for insertion machines are often manually assembled onto semiconductor boards. Solder may also need to be manually applied in difficult-to-reach locations between components. For the latter, delta robots can replace manual operations to place larger components and solder between components.

Delta robots can also be far less costly and far easier to configure than cartesian-type pick-and-place machines. After all, the latter are large and heavy — similar to CNC machine tools. Cartesian systems are difficult to move, and after being moved can require costly and time-consuming recalibration. In contrast, delta robots are small and light enough to relocate fairly frequently. After setup in the new location, they simply run a simple self-calibration routine and then resume operation. Delta robot options abound. Codian Robotics specializes in only delta robots, in contrast with most

we get technical

62

63

Powered by