DigiKey - eMag - Safety - Vol 1

Safety in manufacturing

impractical. They come in a variety of sizes and levels of sensitivity to fit the needs of the manufacturer in meeting OSHA standards. Safety PLCs are a way to program in safeguards in the way that they monitor the health of a line. Through redundancies, the safety PLC is designed to run diagnostics to determine if a part of the line or a component is faulty. If an event such as a broken wire or motor is running outside of spec, the safety PLC will immediately shut down the entire affected system to help prevent injury or damage. The safety PLC must adhere to a specific SIL (safety integrity level) and must meet IEC 62061, ISO 13849-1, and IEC 61058. These are just some of the many safety devices available to manufacturers and installers today. There are many more. When automating a process, it is absolutely necessary to seek advice from a safety expert and consultant to ensure you have covered all of the possible hazards within your facility to protect your workforce and investment. These experts and consultants can help you to navigate OSHA, ANSI, and all other safety regulatory agencies. About the author Eric J. Halvorson is partnership marketing manager II – strategic programs | automation & control at DigiKey.

Door interlocks are another physical safety device commonly integrated on the production floor. Safety interlocks are used on physical barriers such as gates and doors. The Safety interlock, much like the E-Stop, operate in a normally closed circuit. When the gate or door is opened, the circuit is interrupted, and all work is halted. Interlocks are required to meet ISO 14119 and ISO 13849. Another form of safety is an operator presence trigger. These come in many shapes and sizes. For example, in a safety mat. A safety mat is activated by the presence of someone standing on the mat. This can be utilized in a few different ways. It may trigger

a machine to stop, go in reverse or deactivate when presence is detected. This helps to ensure that human workers are out of the way, allowing the machine to operate. Laser safety scanners have become very popular with the rise of cobots. The scanner uses a 360-degree beam that indicates how close a worker or an object are in relation to the robot. Usually with set zones the robot will decrease speed depending upon the closeness of the individual or object. In the orange or yellow zone, the robot is slowed to

collaborative speed until the object or person have exited. If the red zone is triggered, the robot will then slow or even stop completely until safe. Light curtains are especially effective in areas where crushing or pinching hazards exist such as hydraulic presses. The light curtain uses photoelectric beams that project from a transmitter to a receiver. If the beam is broken, all work stops immediately until the obstruction is cleared. Light curtains are particularly effective when solid gates or barricades are

we get technical

6

7

Powered by