DigiKey-emag-Sensors-Vol-7

Understand drone design trade-offs before piling on the sensors

To complement the BMI160, a digital barometric pressure sensor with temperature sensor will help to measure vertical velocity, enhance GPS navigation, and determine a drone’s altitude. It is recommended that barometers be occasionally calibrated at sea level pressures to stay accurate. Bosch Sensortec’s BMP388 barometric pressure and temperature sensor is a good example of an IC that designers can integrate into their architecture. With a small footprint of 2 x 2 mm2 at 0.88 mm high, and a low power consumption of just 3.4 µA at 1 hertz (Hz), this sensor module is well suited for battery operation. The device has a typical relative accuracy of +/-8 Pa with a typical absolute accuracy of +/-50 Pa that will improve drone hovering and obstacle avoidance capabilities. To detect motion along multiple axes, the STMicroelectronics’ ISM330DLCTR iNEMO IMU system- in-package (SiP) module combines an accelerometer and gyroscope along with a magnetometer in a monolithic six-axis IC. This kind of configuration enables a drone to maintain horizontal, vertical, and rotational stability while hovering. For applications like professional- grade drone photography and 3D imagery, six-axis gyro stabilization is necessary and is provided by the ISM330DLCTR.

The gyroscope measures and maintains drone orientation. When integrating three accelerometers, each of which are oriented along a different axis, the degree of motion of a drone along any axis can be determined. This will better enable the collection of information regarding the drone’s roll, pitch, and yaw, and then feed this information back to the drone’s proportional- integral-derivative (PID) controller. The magnetometer will measure the strength and direction of the Earth’s magnetic north field in order to correct its trajectory. Be sure the magnetometer is calibrated frequently; power lines, motors, and any other strong fields emitted from electrical devices can affect it. Drone movement caused by external forces, like a strong gust of wind, will be detected by the accelerometer and relayed to the PID controller, which in turn adjusts the motors to compensate. Rangefinders: Landing, hovering, and distance from an object Drones need to have good sensors to land safely, hover when wirelessly charging, and sense objects to avoid collisions when in motion. This ranging can be performed using sound or light.

Ultrasonic rangefinder sensing: Drone landing, hovering, and ground tracking capabilities can be provided using ultrasonic sensors. When a drone is in the process of landing, it needs to detect the distance from the bottom of the drone to the area in which it is landing. Although GPS and a barometer are part of this control function, accurate distance sensing is the key to a safe landing. Ultrasonic sensors can also assist in safe hovering and ground tracking, which may need the drone to fly at a fixed height. One such distance ranging sensor for landing assistance, hovering, and ceiling detection is MaxBotix ’s MB1010- 000 ultrasonic time-of flight (ToF) ranging sensor board.

Understanding ToF

All of these cases need to use the ToF method, which is the time taken for an emitted ultrasonic wave to reach a target, plus the time for the reflected signal to travel back to the drone’s sensor (Figures 2 and 3). To calculate the distance from the drone to any object, use the equation:

24

Powered by