DigiKey-eMag-Embedded and MCUs-Vol 16

digitized, read into the FPGA, and then some digital signal processor (DSP) algorithms are applied to this signal. Last of all, the FPGA then makes decisions based upon the findings. Such an application will serve as the example throughout this article. Furthermore, Figure 1 illustrates a generic co-processor architecture, where the MCU and FPGA are connected through the MCU’s external memory interface. The FPGA is treated as if it were a piece of external static random-access memory (SRAM). Signals come back to the MCU from the FPGA and serve as hardware interrupt lines and status indicators. This allows the FPGA to indicate critical states to the MCU, such as communicating that an ADC conversion is ready, or a fault has occurred, or another noteworthy event has happened. The strengths of the co-processor approach are probably best seen within the deliverables of each of the above-mentioned milestones. Value is assessed by not only listing the accomplishments of a task or phase but also by assessing the enablement that these accomplishments allow. The answers to the following questions assist in assessing the overall value

Figure 1: Generic co-processor diagram (MCU + FPGA). Image source: CEPD

Microcontroller milestone, the System Management with the Microcontroller milestone, and the Product Deployment milestone. By the conclusion of this article, it will be demonstrated that a flexible hardware architecture can be better suited to modern embedded systems design than a more rigid approach. Furthermore, this approach can result in improvements to both project cost and time to market. Arguments, provided examples, and case studies will be used to defend this position. By observing the value of each milestone within the design flexibility that this architecture provides, it becomes clear that an adaptive hardware architecture is a powerful driver in pushing embedded systems design forward. Exploring the strengths of the co-processor architecture: design flexibility and high- performance processing A common application for FPGA designs is to interface directly with a high-speed analog-to-digital converter (ADC). The signal is

can be harrowing, and yet, they have been spoken and continue to be reinforced throughout the market. What is needed is a design approach, which allows for an evolutionary iterative process to be implemented, and just like with most embedded systems, it begins with the hardware architecture. The co-processor architecture, a hardware architecture known for combining the strengths of both microcontroller unit (MCU) and field programmable gate array (FPGA) technologies, can offer the embedded designer a process capable of meeting even the most demanding requirements, and yet it allows for the flexibility necessary to address both known and unknown challenges. By providing hardware capable of iteratively adapting, the designer can demonstrate progress, hit critical milestones, and take full advantage of the rapid prototyping process. Within this process are key project milestones, each with their own unique value to add to the development effort. Throughout this article, these will be referred to by the following terms: The Digital Signal Processing with the

Written By Noah Madinger, Colorado Electronic Product Design (CEPD) The co-processor architecture: an embedded system architecture for rapid prototyping

Introduction The embedded systems designer finds themselves at a juncture of design constraints, performance expectations, and schedule and budgetary concerns. Indeed, even the contradictions in modern project management buzzwords and phrases further underscore the precarious nature of this role: ‘fail fast’; ‘be agile’; ‘future- proof it’; and ‘be disruptive!’. The acrobatics involved in even trying to satisfy these expectations

Editor’s note: although well known for its digital processing performance and throughput, the co-processor architecture provides the embedded systems designer opportunities to implement project management strategies, which improve both development costs and time to market. This article, focused specifically upon the combination of a discrete microcontroller (MCU) and a discrete field programmable gate

array (FPGA), showcases how this architecture lends itself to an efficient and iterative design process. Leveraging researched sources, empirical findings, and case studies, the benefits of this architecture are explored, and exemplary applications are provided. Upon this article’s conclusion, the embedded systems designer will have a better understanding of when and how to implement this versatile hardware architecture.

of a milestone’s deliverables: ■ Can the progress of other

team members now more rapidly continue, as project dependencies and bottlenecks are removed?

we get technical

10

11

Powered by