DigiKey-eMag-Embedded and MCUs-Vol 16

How to perform firmware updates without halting firmware execution

Figure 2: The PIC32MZ2048EFH144T-I/PH microcontroller has two independent banks of PFM. If SWAP=1, firmware can run out of PFM Bank 1 while PFM Bank 2 is being updated. Clearing SWAP=0 allows the microcontroller to boot out of PFM Bank 2. Image source: Microchip Technology

seven GPR shadow register sets. This significantly improves interrupt performance and context switching by eliminating the many clock cycles required to save the GPRs on the stack. With seven shadow register sets, the core can nest interrupts and context switches seven deep before having to spend clock cycles saving the GPRs on the stack. The PIC32MZ2048EFH144T-I/PH has two 1 Mbyte banks of program flash memory (PFM), designated PFM Bank 1 and PFM Bank 2. Each PFM has its own dedicated boot flash memory (BFM) designated BFM Bank 1 and BFM Bank 2. The BFM does not need to be updated during a PFM update. Having these two separate banks of memory has multiple advantages. For example, the microcontroller supports dual booting, so on power-up it can be configured to boot from either flash memory bank. This allows the microcontroller to support two different device configurations. The two banks of flash also provide the added advantage of allowing firmware execution from one flash bank while updating the firmware in the other flash bank. Microchip refers to this as Live- Update, also referred to as run- time self-programming (RTSP). When RTSP is initiated in an active IoT endpoint executing firmware out of PFM Bank 1, firmware is received over the network in blocks. The recommended method for managing firmware updates over a

Figure 1: The 252 MHz Microchip Technology PIC32MZ2048EFH144T-I/PH is based on the MIPS32 M-Class architecture and has a wide range of serial ports for interfacing to external sensors. Image source: Microchip Technology

additional I2C, SPI, and UART ports as well as general purpose I/O (GPIO) pins on the PIC32MZ EF. There are three pushbuttons and three LEDs that can be configured by firmware. Conclusion IoT sensor endpoints in critical systems are demanding higher memory requirements due to increased code complexity. The more complex the code, the more it is necessary to improve firmware efficiency in order to improve the response times of context switching in the firmware. By selecting a microcontroller that can efficiently run interrupt-driven code that can simultaneously retrieve and update firmware, developers can improve the reliability of critical IoT applications without sacrificing performance. Figure 3: The Microchip Technology DM320007 compact starter kit supports the development and testing of USB and Ethernet applications with the PIC32MZ2048EFH144T-I/PH microcontroller. It includes connectors for USB OTG, USB Host, 10/100 Ethernet, and UART/I2C. Image source: Microchip Technology

network is to store the block of new firmware in SRAM. After receiving a complete block, the firmware executing out of PFM Bank 1 can initiate a programming sequence of the SRAM data into PFM Bank 2. While this firmware is being programmed, firmware execution out of PFM Bank 1 can continue. When the block programming is completed, firmware can request the next block of code over the network and the sequence repeats. This continues until the block of code in PFM Bank 2 is completed. Once the programming is complete, firmware can configure the PIC32MZ2048EFH144T-I/ PH on the next reset to boot from BFM Bank 2 and execute the new firmware in PFM Bank 2 by clearing the SWAP bit in the NVMCON configuration register (Figure 2). If the PIC32MZ2048EFH144T-I/ PH firmware must be updated again while SWAP=0, firmware can execute out of PFM Bank 2 while simultaneously updating PFM Bank 1. The status of the SWAP bit can be changed from either the BFM or the PFM depending upon the needs of the firmware.

Developing dual-boot firmware For development with the PIC32MZ2048EFH144T-I/ PH microcontroller, Microchip Technology provides the DM320007 PIC32MZ starter kit (Figure 3). This board supports multiple serial ports using dedicated connectors as well as header connectors. A USB Host port is used for debugging while a USB OTG port can be used for the application. A USB-to-UART/I2C connector, when connected to a PC USB port, creates a virtual COM port on a connected host PC. This allows the host PC to communicate to the I2C port on the PIC32MZ.

endpoints. Two CAN 2.0b ports allow the microcontroller to network with industrial and automotive networks that use the common CAN protocol. An Ethernet port supports 10/100Base-T networking. A USB 2.0 Hi-Speed controller supports an external interface for additional peripherals or debugging and also supports USB On-The-Go (OTG). Each of these peripherals can generate one or more interrupts. With so many sensors and interrupt sources, maintaining code efficiency becomes a necessity.

To improve efficiency the MIPS32 M-Class CPU core has 32 32- bit general purpose registers (GPRs). This improves efficiency by reducing accesses to external memory. Besides the usual bit set and clear instructions, the M-Class also supports single-cycle bit invert instructions. This improves RTOS efficiency by increasing the efficiency of semaphore handling. The core also has a five-stage instruction pipeline that improves efficiency by minimizing memory access conflicts, resulting in more single-cycle instructions.

A 40-pin expansion header connector allows access to

The MIPS32 M-Class also has

we get technical

52

53

Powered by