DigiKey-emag-Connectors-Vol-11

and external hard drives — to a computer or controller. These connectors are not as common as those used for general use. Products such as the USBCM302M0MICBMMBKR, shown in Figure 2, are used for mobile devices, such as cell phones, tablets, MP3 players, and cameras, as well as portable meters or control units used in industrial settings. The USB Type-B micro allows data to be read without being connected to a computer in applications such as flash drives or memory sticks connected directly

to a device. Similar to the Type-A connectors, these devices only go into a port one way and can be damaged if not done so. The newest connector device is the USB Type-C. These connectors and cables, such as the USBCM311M0USBCMMMWHR shown in Figure 3, are designed specifically for high-speed data transfer and higher current flow, allowing devices to charge more quickly. Unlike other USB Type connectors, the USB Type-C can be plugged into a device in either direction.

Figure 3: The USBCM311M0USBCMMMWHR is a shielded, 1-meter-long, USB-C male to USB-C male cable capable of handling 10Gbps data rates. (Image source: GlobTek, Inc.)

Conclusion

USB connectors and cable assemblies are an integral part of everyday life. These assemblies have made it into almost every home to interconnect laptop and desktop computers to multiple peripherals, as well as for connecting mobile phones and tablets to power sources. USB components are also used in automation, where high-speed data transfer between computers and remote sensors and transducers is essential. GlobTek’s certifications and commitment to quality position them as a dependable source capable of meeting the demands of consumers and manufacturers alike.

Figure 2: The USBCM302M0MICBMMBKR, USB Type-B micro male plug to Type-C male plug with 2.00 meter shielded cable shown, is often used to connect devices directly to flash drives or memory sticks without needing to connect through a computer. (Image source: GlobTek, Inc.)

we get technical

83

Powered by