DigiKey-emag-MedTech-Vol-12

IEC 60601-1-8 guidance for designing medical equipment alarms

With buzzers, you also have the possibility to customize their output so that a buzzer can, without any special driver, create the precise tone required by IEC 60601-1-8. Same Sky has created an array of medical buzzers that not only meet the audio requirements set out by the guidelines but also meet the robustness requirements outlined. The tones available are identified in IEC 60601-1-8 and correspond to the more common concerns found in the medical industry (click the links below to listen to the specific tones): ■ Cardiovascular, which sounds somewhat like a heart beating ■ Oxygen , which sounds similar to a dripping noise ■ Ventilation, which sounds like someone breathing ■ General , which is a more generic sound

Conclusion Medical equipment is and will continue to be in great demand and expectations will also continue to rise. Fortunately, with clear and detailed instructions, the IEC 60601-1-8 standard codifies and simplifies the alarm aspect of medical equipment. While intense and potentially daunting, properly done, audible medical alarms can significantly increase the effectiveness of equipment and potentially save lives. To decrease the barrier to entry and any difficulty in implementing these guidelines, Same Sky has created medical buzzers and speakers that meet IEC 60601-1-8 requirements. For more explicit detail about IEC 60601-1-8, you can purchase the official document on the IEC website at www.iec.ch.

Medical equipment is and will continue to be in great demand and expectations will also continue to rise. Fortunately, with clear and detailed instructions, the IEC 60601-1- 8 standard codifies and simplifies the alarm aspect of medical equipment.

Figure 1: Same Sky buzzer designed for medical applications. Image source: Same Sky

for unexpected noise. Properly sized capacitors can absorb high frequency noises if they do not interfere with the intended signal. Physically protecting the connections from potentially coming into contact with outside electrical sources, including static electricity, will also help with this concern. Overall, while speakers are more of a challenge and require more thought in their implementation, they are an excellent choice when extra flexibility is needed. Same Sky has also developed specific medical speakers designed to meet the IEC 60601-1-8 guidelines.

Speakers versus buzzers in medical equipment While IEC 60601-1-8 is focused on the sounds, the waveforms, and where the buzzers are used, it does not provide significant direction on what exactly should be used nor where it should be placed. While there are many benefits to buzzers, and they work in a wide range of applications, as mentioned earlier in this article, there are other options. While not as energy efficient as buzzers and more difficult to drive, speakers offer almost limitless flexibility in the sounds they make. Fully human voices, music, and any mixture of sounds, even at the same time, are all possible using a standard speaker. There are directions in IEC 60601-1- 8 about how speakers tend to make popping noises when there are sudden voltage changes, like when old headphones were plugged into a receiver or computer. While shaping the noise waveforms, you can avoid any sharp changes that would cause these noises, however, you will need to account

While this standard originated in the European Union, it is mandatory not only in the EU but also in the US and Canada. This is hugely beneficial for product designers to promote simpler compliance in multiple major locations and improves device safety and performance across the globe. Medical alarm systems part selection There are many components that can be used for the audio portions of a medical device. Sirens, buzzers, and even bells can be used, though other transducers are very common as well. These components are not equal and vary significantly in the difficulty of implementation, cost, power consumption, and flexibility. Electrical buzzers check the boxes in terms of cost, ease of implementation, flexibility, and power efficiency. Buzzers are unique because they either use electromechanical drivers, sometimes referred to as magnetic

buzzers, or piezoelectric drivers, using a ceramic piezo driver. Because of these options, you can get different voltages, frequency ranges, sound pressure levels, footprints, and more, making buzzers the ideal choice for many alarms. In particular, Piezo buzzers are known for creating a louder signal (larger sound pressure level) than their electromechanical counterparts for the power consumed.

Figure 2: Sample waveforms of specific medical device tones. Image source: Same Sky

we get technical

44

45

Powered by