DigiKey-eMag-EdgeAI-Vol 18

How to build an AI-powered toaster

Machine learning model training Clone this Edge Impulse project as a starting point: studio. edgeimpulse.com/public/129477/ latest If you wish to use your own data, delete all of the data in the project and upload the data from the unzipped out.zip file. Note that you should upload files in the training/ directory to training in Edge Impulse and upload files in testing/ to testing. Go to Raw data. Click Save parameters and then Generate features. When that’s done, go to Regression. Feel free to modify the model, if you’d like. Click Start training and wait for training to finish. Go to Model testing and click Classify all. When that’s done, you should see some estimates. Expected outcome is the ground- truth label that expresses the number of seconds until the toast is burned, which is calculated based on when the state label transitioned from ‘toasting’ to ‘burnt’ (0 being the moment we believe the toast went from ‘toast’ to ‘burnt toast’). The result is the output of our model, given the test input data. For the most part, the model is capable of predicting ‘time till burnt’ within a few seconds. Interestingly, the model seems to be more accurate the closer to 0.

or burnt. Use your senses (sight, smell) to determine when you think the toast is ‘burnt’. See the CSV files in the datasets/ directory to see how I labeled the raw data. You’re welcome to use that data as a starting point (I just can’t promise that it will give you a model that works in your environment). Each folder is the brand, and a description of the bread used. The prefix of each CSV file is where I pulled the bread from (e.g. room temperature, refrigerator, freezer).

Data curation

Recommended reading All code in this project can be found in this GitHub repository. The Edge Impulse project used for training the machine learning model is found here. Interestingly enough, creating the perfect toast is an exercise in predictive maintenance. Instead of ‘toast’, imagine we’re talking about an expensive piece of machinery. Is it possible to create a system that predicts when the machinery will fail (analogous to the toast burning) and notify us before it does fail (e.g. stopping the toasting process just before burning)? Performing routine maintenance might help limit or prevent machine failure, but it is often done more than necessary, which increases equipment downtime. Predictive maintenance systems help limit this downtime by notifying us before a machine breaks so we can repair it at the appropriate times. You can read more about predictive maintenance in this blog post.

Run this notebook in Google Colab, following all of the directions: github.com/ShawnHymel/perfect- toast-machine/blob/main/ptm_ dataset_curation.ipynb Note that the script will automatically download the dataset from the GitHub directory. You can skip those cells and manually upload your data to the dataset/ folder in Colab if you wish to use your own data. At the end of Step 2, you can view plots of your captured raw gas samples (one at a time). Blue is ‘background’, green is ‘toasting’, and red is ‘burnt’. At the end of Step 3, you should see means, standard deviations, minimums, and ranges printed out. Copy those down – you’ll need the means and standard deviations for your inference code. Step 4 will produce an out.zip file containing your curated dataset. Download this file and unzip it.

Copy the means and standard deviations from the Colab script to the means and std_devs arrays, respectively. The first time you try the project, pay attention to the number displayed on the Wio Terminal. This shows the number of predicted seconds until the toast is burned. If your toast comes out to light, lower the CANCEL_THRESHOLD in the code (i.e. wait until it is closer to being burned before popping the toast up). If the toast is too dark, increase the CANCEL_THRESHOLD (i.e. stop the toasting process sooner). With a little tweaking, you should be able to make perfect toast! Try different types of bread, different thicknesses, different starting temperatures, etc. It should also work for two slices of bread and even bagels!

Deployment

Go to the Deployment page, select Arduino library, and click Build. When the library has been downloaded (do not unzip it!) open the Arduino IDE, click Sketch > Include Library > Add .ZIP Library … select the Arduino library that you just downloaded from Edge Impulse. Note the name of the library! If it is different than ei- perfect-toast-machine-arduino- x.x.x.zip, you will need to change the .h include file name in your inference code. Copy the perfect-toast-machine Arduino code found here to a new Arduino project. Read the comments at the beginning to see which libraries you need to install. Rename perfect-toast- machine_inferencing.h if you used a different project name in Edge Impulse. Upload the code to your Wio Terminal.

we get technical

20

21

Powered by