Road-tested GMSL cameras drive into new markets
through the same cable: GMSL uses Power over Coax (PoC) so video, audio, control, data, and power can be transported on a single channel. Most GigE Vision applications rely on Power over Ethernet (PoE) for 4-pair Ethernet, or less commonly, Power over Data Line (PoDL) for Single-Pair Ethernet (SPE). System requirements and application needs will determine which vision technology is most appropriate. GigE Vision, for example, may offer some advantages for single-camera applications, particularly where they connect directly to a PC or an embedded platform with an Ethernet port. When using multiple cameras, GigE Vision applications will require use of a dedicated Ethernet switch, a network interface card (NIC) with multiple Ethernet ports, or an Ethernet switch IC. That switching requirement can potentially reduce the maximum total data rate and introduce unpredictable latency between the cameras and the terminal device, whereas GMSL provides a simpler, more direct architecture.
GigE Vision devices may support higher resolution and a higher frame rate – or both simultaneously – with additional buffering and compression. Frame buffering and processing are not provided by GMSL devices, so resolution and frame rate depend on what the image sensor can support within the link bandwidth. Engineers will need to determine a simple trade- off between resolution, frame rate, and pixel bit depth. GMSL simplifies high-speed video architecture GigE Vision cameras typically utilize a signal chain that includes an image sensor, a processor, and an Ethernet physical layer (PHY) (Figure 1). Raw image data from the sensor is converted by the processor into Ethernet frames, often relying on compression or frame buffering to fit the data rate of the supported Ethernet bandwidth. The GMSL camera signal chain utilizes a serializer/deserializer (SerDes) architecture that avoids the use of a processor (Figure 2). Instead, image sensor parallel data is converted by the serializer into
a high-speed serial data stream. On the back end, a deserializer converts the serial data back into parallel form for processing by an electronic control unit (ECU) system-on-chip (SoC). The GMSL camera architecture makes it simpler to design small form factor cameras with low power consumption. Serializers can directly connect to cameras through standard MIPI CSI-2 interface and transmit packetized data through the GMSL link. A typical host device is a customized embedded platform with one or more deserializers that transmit image data through MIPI transmitters in the same format as the image sensor MIPI output. New GMSL camera drivers are required for customized designs, but if there is an existing driver for the image sensor, it can be utilized with just a few profile registers, or register writes to enable a video stream from cameras to a control unit.
Figure 2: GMSL cameras utilize a simpler signal chain architecture on the sensor side than GigE Vision. Image source: Analog Devices, Inc.
application needs, such as device interfaces, data rates, bandwidth, power consumption, environmental conditions, and cable length. Other factors include EMI, error handling, and signal integrity. Some examples of ADI’s GMSL components include: ■ MAX96717, a CSI-2 to GMSL2 serializer (Figure 3), operates at a fixed rate of 3 Gbps or 6 Gbps in the forward direction and 187.5 Mbps in the reverse direction ■ MAX96716A , which converts dual GMSL2 serial inputs to MIPI CSI-2. The GMSL2 inputs operate independently and video data from both can be aggregated for output on a single CSI-2 port or replicated on a second port for redundancy ■ The MAX96724 , a quad tunneling deserializer, converts four GMSL 2/1 inputs to 2 MIPI D-PHY or C-PHY outputs. Data link rates are 6/3 Gbps for GMSL2 and 3.12 Gbps for GMSL1, and reverse link rates of 187.5 Mbps for GMSL2 and 1 Mbps for GMSL1 ■ The MAX96714 deserializer converts a single GMSL 2/1 input to MIPI CSI-2 output, with a fixed rate of 3 Gbps or
6 Gbps in the forward direction and 187.5 Mbps in the reverse direction ■ The MAX96751 is a GMSL2 serializer with HDMI 2.0 input that converts HDMI to single or dual GMSL2 serial protocol. It also enables full-duplex, single- wire transmission of video and bidirectional data ■ The MAX9295D converts single- or dual-port 4-lane MIPI CSI-2 data streams to GMSL2 or GMSL1 ADI also offers several development tools, such as the MAX96724-BAK-EVK# evaluation kit for the MAX96724 devices.
Conclusion
With their reduced complexity, GMSL cameras are more compact and generally able to provide a more cost-effective solution compared to GigE Vision. GMSL provides reliable transport of high-resolution digital video with microsecond latency for a growing range of camera and display-based applications, from machine learning and autonomous operations to infotainment and safety. Millions of GMSL links are enhancing the driver experience on the road today, attesting to their reliability and performance.
GMSL components ADI offers a comprehensive portfolio of serializers and
deserializers to support a variety of interfaces. These feature robust PHY designs, low bit error rates (BER), and backward compatibility. Any video protocols can be bridged together – for example, HDMI to the Open LVDS Display Interface (oLDI). Engineers will need to select the best components based on
Figure 3: A schematic illustrating the data stream utilizing MAX96717 serializers. Image source: Analog Devices, Inc.
Figure 1: Representation of key signal chain components on the sensor side of GigE Vision cameras. Image source: Analog Devices, Inc.
we get technical
38
39
Powered by FlippingBook